| Leaflet |
Doc No: AD12 Title: Application notes - AC drives enable precise gas fl ow and
reduce energy consumption of cement ID fans - Fact File Revision: B Part: 1 File type: pdf Summary: For cement quality, the operation of the ID fan plays a very important role. The ID fan sucks air through the kiln and through the preheater tower. When burning, the mix of air and fuel turns into gas. The burning temperature inside the kiln and the temperature in the preheater tower cyclones are kept constant. FactFile Cover page: ![]() Application notes - AC drives enable precise gas fl ow and
reduce energy consumption of cement ID fans - Fact File | English
| 0.19 MB |
Doc No: 9AKK104295D7691 Title: Application notes - AC drives ensure efficient and precise cooling of clinker and reduce energy consumption - Fact File Revision: A File type: pdf Summary: Clinker cooling is best carried out by controlling each cooling fan and exhaust aire fan motor separately using AC drives. FactFile, Fact File Cover page: ![]() Application notes - AC drives ensure efficient and precise cooling of clinker and reduce energy consumption - Fact File | English
| 0.19 MB |
Doc No: AD11 Title: Application notes - AC drives improve cement kiln control and
reduce energy consumption - Fact File Revision: B Part: 1 File type: pdf Summary: The kiln is the most critical element in the cement making process. It is where the chemical processes occur that turn raw mix into clinker. The kiln also consumes the greatest amount of energy (fuel plus electricity)
within a cement plant. FactFile Cover page: ![]() Application notes - AC drives improve cement kiln control and
reduce energy consumption - Fact File | English
| 0.18 MB |
Doc No: CD18 Title: Case Notes - ABB drive boosts sugar centrifuge production and uptime - Fact File Revision: A Part: 1 File type: pdf Summary: ABB regenerative drive provides savings and increases throughput at Sugar Cane Growers prosessing plant in USA. The drive provides precise , rapid motor-speed response based on exact variations of the centrifuge load. Cover page: ![]() Case Notes - ABB drive boosts sugar centrifuge production and uptime - Fact File | English
| 0.09 MB |
Doc No: CD27 Title: Case notes - ABB drives and remote monitoring reduce costs in wastewater pumping system - Fact File Revision: A Part: 1 File type: pdf Summary: Increasing wastewater treatment requirements prompted Larsmo municipality in Finland to take action to combat the problem of stormwater leakage into its sewer system. Two of Larsmo's 15 wastewater pumping stations have been upgraded with ABB industrial drives - both having two drives in master/follower configuration - and intelligent pump control (IPC) software. One upgraded pumping stations is equipped with ABB's intelligent ethernet module, NETA-01, for remote access, monitoring and real time diagnostics. Fact File, FactFile Cover page: ![]() Case notes - ABB drives and remote monitoring reduce costs in wastewater pumping system - Fact File | English
| 0.55 MB |
Doc No: CD23 Title: Case notes - ABB drives boost efficiency of sewage pumping station - Fact File Revision: C Part: 1 File type: pdf Summary: EMAYA SA, the water supply and waste utility for the Spanish city of Palma de Mallorca, recently launched a project to upgrade its wastewater pumping stations. Four 60 kW submersible pumps have been installed at the first station. Each pump is opearated by an ABB industrial drive running intelligent pump control (IPC) software. Fact File, FactFile Cover page: ![]() Case notes - ABB drives boost efficiency of sewage pumping station - Fact File | English
| 0.12 MB |
Doc No: CD33 Title: Case notes - ABB drives cut energy costs of multiple fans by 30% at Castle Cement - Fact File Revision: - Part: 1 File type: pdf Summary: Variable speed control by means of AC drives is the most cost-effective way to control the gas flow. Through variable speed control, maintenance costs at Castle Cement are considerably reduced. Fact File. FactFile Cover page: ![]() Case notes - ABB drives cut energy costs of multiple fans by 30% at Castle Cement - Fact File | English
| 0.22 MB |
Doc No: CD32 Title: Case notes - ABB drives ensure high cement quality for Europe's most modern kiln - Fact File Revision: A Part: 1 File type: pdf Summary: Two ABB industrial drives are saving energy, ensuring the quality and increasing the quantity of cement produced by Europe's most modern, 65 metre long cement kiln at Castle Cement's Padeswood works in north Wales, UK. Fact File. FactFile Cover page: ![]() Case notes - ABB drives ensure high cement quality for Europe's most modern kiln - Fact File | English
| 0.21 MB |
Doc No: CD16 Title: Case Notes - ABB drives maintain stable pressure in municipal water supply - Fact File Revision: A Part: 1 File type: pdf Summary: The drives at the pressure boosting station are provided with intelligent pump control (IPC), an optional software for ABB's industrial drives which incorporates all the functions generally required by pump users. In this case the functions used are multipump control, pump priority, and flow measurement. FactFile Cover page: ![]() Case Notes - ABB drives maintain stable pressure in municipal water supply - Fact File | English
| 0.08 MB |
Doc No: CD46 Title: Case Notes - ABB drives save £25,000 on energy at duck processing plant - Fact File Revision: B Part: 1 File type: pdf Summary: Cherry Valley Farms is the largest manufacturer of duck and duck products in the U.K.. The chilling plant is a major part of the factory's operation and accounts for a high proportion of its operating cost. FactFile, Fact File Cover page: ![]() Case Notes - ABB drives save £25,000 on energy at duck processing plant - Fact File | English
| 0.15 MB |
Doc No: CD5 Title: Case Notes - AC drives in ski lift applications at Breckenridge and Sugarbush - Fact File Revision: A Part: 1 File type: pdf Summary: ABB's industrial drives are used in ski lifts in Colorado and Vermont, USA. The promise of a significant reduction in power consumption and maintenance free motor operation for large, high-power chairlift operations led the ski resorts to install regenerative AC drives and motors. FactFile, Fact File Cover page: ![]() Case Notes - AC drives in ski lift applications at Breckenridge and Sugarbush - Fact File | English
| 0.06 MB |
Doc No: CD35 Title: Case Notes - DSM's research facility saves 25, 000 Euros a year with ABB standard drives for HVAC - Fact File Revision: B Part: 1 File type: pdf Summary: FactFile, Fact File Cover page: ![]() Case Notes - DSM's research facility saves 25, 000 Euros a year with ABB standard drives for HVAC - Fact File | English
| 0.13 MB |
Doc No: CD21 Title: Case notes - Energy centre 14 percent more efficient with variable speed drives - Fact File Revision: B Part: 1 File type: pdf Summary: Heinz' energy centre in the UK is 14 percent more efficient by using ABB standard drives. Fact File, FactFile Cover page: ![]() Case notes - Energy centre 14 percent more efficient with variable speed drives - Fact File | English
| 0.14 MB |
Doc No: CD2 Title: Case Notes - Flooring company saves £15,000 annually in electricity bills - Fact File Revision: A Part: 1 File type: pdf Summary: Cooling tower pump pressure reduced from 120 to 80 bar with variable speed drive. Fact File, FactFile Cover page: ![]() Case Notes - Flooring company saves £15,000 annually in electricity bills - Fact File | English
| 0.22 MB |
Doc No: CD12 Title: Case Notes - Low harmonics reduce costs of blown film production - Fact File Revision: B Part: 1 File type: pdf Summary: Idealplast in Italy needed a very low harmonic level in order to optimise the calculated cost for each kilogram of film produced. ABB industrial drives improve production process. Fact File, FactFile Cover page: ![]() Case Notes - Low harmonics reduce costs of blown film production - Fact File | English
| 0.27 MB |
Doc No: CD45 Title: Case notes - McDonald's save 50% on fan power with ABB standard drive for HVAC - Fact File Revision: B File type: pdf Summary: McDonald's was updating cooking equipment in a number of its restaurants across the UK. During the project McDonald's realized it could reduce its carbon footprint by making large fans run more slowly. The company decided to use a low voltage AC drive to achieve the slower fan control. Fact File.FactFile Cover page: ![]() Case notes - McDonald's save 50% on fan power with ABB standard drive for HVAC - Fact File | Swedish
| 0.24 MB |
Doc No: CD45 Title: Case notes - McDonald's save 50% on fan power with ABB standard drive for HVAC - Fact File Revision: A File type: pdf Summary: McDonald's was updating cooking equipment in a number of its restaurants across the UK. During the project McDonald's realized it could reduce its carbon footprint by making large fans run more slowly. The company decided to use a low voltage AC drive to achieve the slower fan control. Fact File.FactFile Cover page: ![]() Case notes - McDonald's save 50% on fan power with ABB standard drive for HVAC - Fact File | English
| 0.18 MB |
Doc No: CD48 Title: Case Notes - Refrigeration energy costs set to reduce by £6,000 with ABB drives - Fact File Revision: A File type: pdf Summary: The installation of a new production line, complete with spiral freezer, designed for the manufacture of a variety of puff pastry products, prompted Poole's Pies in the UK to look at its energy efficiency. FactFile, Fact File Cover page: ![]() Case Notes - Refrigeration energy costs set to reduce by £6,000 with ABB drives - Fact File | English
| 0.24 MB |
Doc No: CD20 Title: Case notes - Salt producer saves £100,000 on single fan - Fact File Revision: B Part: 1 File type: pdf Summary: Salt Union has the capacity to produce a million tonnes of salt every year at its site in Runcorn, Cheshire. An energy survey by ABB Drives Alliance member Central Electrical was carried out to determine what potential saving could be achieved. Costing just £20k, the ABB equipment installed is saving over £100k a year, representing a cut in energy consumption of over 60 percent. FactFile Cover page: ![]() Case notes - Salt producer saves £100,000 on single fan - Fact File | English
| 0.20 MB |
Doc No: CD34 Title: Case notes - School cuts energy costs using ABB standard drives for HVAC - Fact File Revision: B Part: 1 File type: pdf Summary: ABB standard drives for HVAC reduced electricity consumption at Konala Comprehensive School in Finland by 14% during the first 10 months of operation while the heating used fell by 16 %. Fact File.FactFile Cover page: ![]() Case notes - School cuts energy costs using ABB standard drives for HVAC - Fact File | Swedish
| 0.62 MB |